ECAT.USEPLL

Description

This parameter configures the usage of the PLL when the EtherCAT-master uses only the SYNC manager events to synchronize the EtherCAT slaves.

Value Description
0 Off - Not synchronized
1 Synchronize without using Distributed Clock (synchronizes to the EtherCAT cyclic [SYNC manager] messages)

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

EtherCAT drives: AKD2G-SPE

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ECAT.USEPLL

4300h

06h

Unsigned8

-

-

Read/Write

No